Captures the high/low-level width measured between pulses of the signal (pulses) input to the TImn pin.
[Syntax]
#include “r_cg_macrodriver.h”
void R_TAUm_Channeln_Get_PulseWidth ( uint32_t * const width );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
Unit32_t * const width; |
Pointer to an area to store the measurement width (0x0 to 0x1FFFF) |
[Return value]
None.