Reads the pulse width of the 16-bit timer RDn.
Remark 1. This API function can only be called when the 16-bit timer RDn is being used for input capture function.
Remark 2. If there is an overflow (2 pulses or more) during pulse-width measurement, then the pulse width will not be read correctly.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_timer.h”
MD_STATUS
R_TMRDn_Get_PulseWidth ( uint32_t * const
active_width,
uint32_t * const inactive_width, timer_channel_t
channel );
Remark n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
unit32_t * const active_width; |
Pointer to an area storing the active level width that was read |
|
O |
uint32_t * const inactive_width; |
Pointer to an area storing the inactive level width that was read |
|
I |
timer_channel_t channel; |
in to read TMCHANNELA : TRDIOAn pin TMCHANNELB : TRDIOBn pin TMCHANNELC : TRDIOCn pin TMCHANNELD : TRDIODn pin |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |