Performs processing in response to detection of overrun error.
Remark This API function is called as the callback routine of interrupt process r_uartn_interrupt_receive corresponding to the UART reception end interrupt INTSRn (process performed when the amount of data received is greater than the argument rx_num specified for R_UARTn_Receive ).
[Syntax]
#include “r_cg_macrodriver.h”
static void r_uartn_callback_softwareoverrun ( uint16_t rx_data );
Remark n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
O |
uint16_t rx_data; |
Receive data (greater than the argument rx_num specified for R_UARTn_Receive) |
[Return value]
None.