Usage example
Start clock and buzzer output
[GUI setting example]
|
Clock output/Buzzer output |
Used | |||
|
PCLBUZ0 |
Used | |||
|
Clock output/buzzeroutput operation setting |
Used | |||
|
PCLBUZ0 output clock selection |
1.875 (fSL/2^3)(kHz) | |||
|
Slow mode |
Unused | |||
[API setting example]
r_main.c
void main(void)
{
R_MAIN_UserInit();
/* Start user code. Do not edit comment generated here */
/* Start the PCLBUZ0 module */
R_PCLBUZ0_Start();
while (1U)
{
;
}
/* End user code. Do not edit comment generated here */
}