Everything

R_CGC_Set_ClockMode

Sets the clock source.

 

[Syntax]

#include       "r_cg_macrodriver.h"

#include       "r_cg_cgc.h"

MD_STATUS   R_CGC_Set_ClockMode ( clock_mode_t mode );

 

[Argument(s)]

I/O

Argument

Description

I

clock_mode_t mode;

Clock source type

MAINCLK            : Main clock oscillator

SUBCLK              : Sub-clock oscillator

PLLCLK               : PLL circuit

HOCO                  : High-speed on-chip oscillator

LOCO                   : Low-speed on-chip oscillator

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ERROR1

Exit with error (abend)

MD_ARGERROR

Invalid argument mode specification