Everything

r_cmpb_cmpbn_interrupt

Performs processing in response to the comparator B interrupt.

Remark         This API function is called to run interrupt processing for the comparator Bn interrupt, which is generated when the comparison result changes at this time.

 

[Syntax]

static void    r_cmpb_cmpbn_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.