Everything

r_cmtw_icmin_interrupt

Performs processing in response to the input capture interrupt.

 

[Syntax]

static void    r_cmtw_icmin_interrupt ( void );

Remark         m is the timer general register number, n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.