Everything

r_lvd_lvdn_interrupt

Performs processing in response to the voltage monitoring n interrupt.

Remark         This API function is called to run interrupt processing for the voltage monitoring n interrupt, which is generated when the voltage detection circuit detects the voltage being dropped.

 

[Syntax]

static void    r_lvd_lvdn_interrupt ( void );

Remark         n is the circuit number.

 

[Argument(s)]

None.

 

[Return value]

None.