Everything

r_poe3_oein_interrupt

Performs processing in response to the output enable interrupt.

Remark         This API function is called to run interrupt processing for the output enable interrupt, which is generated when a related pin becomes high-impedance or the output short flag 1 is set.

 

[Syntax]

static void    r_poe3_oein_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.