Performs processing in response to the A/D scan end interrupt.
Remark This API function is called to run interrupt processing for the A/D scan end interrupt, which is generated on completion of scanning of the analog inputs.
[Syntax]
static void r_s12adn_interrupt ( void );
Remark n is the unit number.
[Argument(s)]
None.
[Return value]
None.