Everything

vrst_mbx

Outline
Reset mailbox.
C format
 ER      vrst_mbx (ID mbxid);
Parameter(s)
I/O
Parameter
Description
I
 ID      mbxid;
ID number of the mailbox.

Explanation
This service call reset the mailbox specified by parameter mbxid.
The messages having been accumulated by the mailbox come off from the management of the RI600PX.
Note 1 In this service call, the tasks to wait to receive message do not released from the WAITING state.
Note 2 This service call is the function outside mITRON4.0 specification.
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- mbxid < 0
- mbxid > VTMAX_MBX
E_CTX
-25
Context error.
- This service call was issued from a non-task.
- This service call was issued in the CPU locked state.
- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
E_MACV
-26
Memory access violation.
- Stack pointer points out of user stack for invoking task.
E_NOEXS
-42
Non-existent object.
- The mailbox specified by mbxid does not exist.