|
|
Select trace mode of Realtime OS Task Analyzer
|
|
|
Taking in trace chart by hardware trace mode
|
|
|
Select from the drop-down list.
|
|
|
|
Can not use Realtime OS Task Analyzer
|
Taking in trace chart by hardware trace mode
|
The trace information is collected in the trace memory which emulator or simulator has.
|
Taking in trace chart by software trace mode
|
The trace information is collected in the trace buffer secured on the user memory area.
To use this mode, implementation of user-own coding module and setup of the system configuration file are required. For details, refer to chapter 15.3.1.
|
Taking in long-statistics by software trace mode
|
The trace information is collected in the RI600V4's variable secured on the user memory area.
To use this mode, implementation of user-own coding module and setup of the system configuration file are required. For details, refer to chapter 15.3.2.
|
Operation after used up the buffers
|
Select the operation after user up the trace buffer.
This item is displayed only when "Taking in trace chart by software trace mode" is selected.
|
|
|
Continue to exection while the buffers overwriting
|
|
|
Select from the drop-down list.
|
|
|
Continue to exection while the buffers overwriting
|
It is overwritten sequentially from old information.
|
|
|
The RI600V4 stops tracing.
|
|
|
This item is displayed only when "Taking in trace chart by software trace mode" is selected.
|
|
|
|
|
|
Directly enter to the text box. Only a hexadecimal number can be entered.
|
|
|
|
|
|
This item is displayed only when "Taking in trace chart by software trace mode" is selected.
|
|
|
|
|
|
Select from the drop-down list.
|
|
|
|
The trace buffer with the specified size is generated in the BRI_TRCBUF section when building.
|
|
|
The buffer address is specified by the following clause.
|
|
|
Specify the start address of the "Another buffer" by immediate value.
Area with "Buffer size" (bytes) from "Buffer address" is used as the trace buffer. Please be careful not to overlap with other program or data area.
This item is displayed only when "Another buffer" is selected.
|
|
|
|
|
|
Directly enter to the text box. Only a hexadecimal number can be entered
|
|
|
From 0x0 to 0xFFFFFFFF, and "Buffer address" + "Buffer size" must not exceeds 0xFFFFFFFF.
|