rel_mpf
irel_mpf
ER rel_mpf (ID mpfid, VP blk);
ER irel_mpf (ID mpfid, VP blk);
 This service call returns the fixed-sized memory block specified by parameter blk to the fixed-sized memory pool specified by parameter mpfid.
 If a task is queued to the target fixed-sized memory pool wait queue when this service call is issued, fixed-sized memory block return processing is not performed but fixed-sized memory blocks are returned to the relevant task (first task of wait queue).
 As a result, the relevant task is unlinked from the wait queue and is moved from the WAITING state (WAITING state for a fixed-sized memory block) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.