tget_mpl
ER tget_mpl (ID mplid, UINT blksz, VP *p_blk, TMO tmout);
 This service call acquires a variable-size memory block of the size specified by parameter blksz from the variable-size memory pool specified by parameter mplid, and stores its start address into the area specified by parameter p_blk.
 If no variable-size memory blocks could be acquired from the target variable-size memory pool (no successive areas equivalent to the requested size were available) when this service call is issued, this service call does not acquire variable-size memory blocks but queues the invoking task to the target variable-size memory pool wait queue and moves it from the RUNNING state to the WAITING state with time-out (variable-size memory block acquisition wait state).
| 
 The variable-size memory block that satisfies the requested size was returned to the target variable-size memory pool as a result of issuing rel_mpl. | |
 Note 2	 Invoking tasks are queued to the target variable-size memory pool wait queue in the FIFO order.
 Note 4	 The alignment number of memory blocks is 1. To enlarge the alignment number to 4, specify unique section to Section name assigned to the memory pool area (mpl_section) in Variable-sized Memory Pool Information (variable_memorypool[]) and locate the section to 4-bytes boundary address when linking.
 Note 5	 TMO_FEVR is specified for wait time tmout, processing equivalent to get_mpl will be executed. When TMO_POL is specified, processing equivalent to pget_mpl will be executed.