-   
 
   vrst_mbx
  
    -   
  
 
 ER      vrst_mbx (ID mbxid);
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 ID      mbxid;
 
 | 
    
 ID number of the mailbox.
  
 | 
  
 
 This service call reset the mailbox specified by parameter 
mbxid.
 
 The messages having been accumulated by the mailbox come off from the management of the RI600V4.
 
 Note 1	 In this service call, the tasks to wait to receive message do not released from the WAITING state.
 
 Note 2	 This service call is the function outside 
mITRON4.0 specification.
 
 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 | 
  
  
    | 
 | 
    
 | 
    
 -	 This service call was issued from a non-task.
  
 -	 This service call was issued in the CPU locked state.
  
 -	 This service call was issued in the status "PSW.IPL > kernel interrupt mask level".
  
 |