Everything

13.3.3 Clock timer interrupt source

Define the following items as clock timer interrupt source information:
Only one information item can be defined as clock timer interrupt source information
The following shows the clock timer interrupt source information format.
 CLK_INTNO ( tim_intno );

The items constituting clock timer interrupt source information are as follows.
1 ) Clock timer interrupt source: tim_intno
Specifies the interrupt source for a clock timer.
Only interrupt source names prescribed in the device file or only values from 0x0 to 0x7c can be specified.
If an interrupt source name is specified for tim_intno, the CF78V4 activation option -cpu D <name> must be
specified.