|
-pirod [V1.07.00 or later]
|
This option enables the PIROD facility.
[Specification format]
- | Interpretation when omitted |
The PIROD facility is disabled.
[Detailed description]
- | When this option is specified, the relocation attribute that can be specified in the .cseg or .section directive is changed. |
If a relocation attribute shown below is specified, an error will occur.
When this option is specified: CONST, ZCONST, or ZCONST23
When this option is not specified: PCCONST16, PCCONST23, or PCCONST32
- | When this option is specified, the predefined macro __PIROD will be valid. |
- | If this option is not specified simultaneously with the -pic option, an error will occur. |
- | This option only controls the relocation attribute that can be specified. The processing for determining whether there is an error in the code for referencing constant data is not performed. |