This option specifies whether to use the arithmetic unit.
When the -cpu=S1 or -cpu=S3 option is specified, the code is the same as when the -use_mda=not_use option is specified.
When the -cpu=S2 option is specified, the code is the same as when the -use_mda=mda option is specified.
This option only specifies the instruction set and architecture and does not specify whether the division/multiplication and multiply-accumulate unit is implemented. |
To generate a code that uses the division/multiplication and multiply-accumulate unit, describe as: |