Everything
5.1.9 Byte separation operators

The following byte separation operators are available.

Operator

Overview

HIGH

Obtains the second byte from the least significant byte of a term

LOW

Returns the low-order 8-bit value of a term