Everything
11.2.8 Specifying standard library functions when C99 standard is specified by an individual option

When calling standard library functions complying with the C99 standard from a source program based on the C99 standard with the C99 standard specified individually by the -lang option, use a link option to specify usage of the standard library functions for the C99 standard.