This section describes how to enable the debugging facilities for the initial stop state or standby mode and gives notes on usage when the selected microcontroller is in the initial stop state or incorporates a specific standby-mode facility.
In some descriptions, this section refers to the states of the microcontroller listed below as well as those in the Main window.
|
The state of cores other than the main core when the main core is in the cyclic run mode or cyclic stop mode |
Set the following for debugging the initial stop state or standby mode.
The [Connection with Target Board] category on the [Connect Settings] tab in the Property panel
If this facility is not used, a program that includes a transition to standby mode cannot be debugged. |
In asynchronous debugging mode, the following method is available but is restricted to the initial stop state. |
Execute after resetting microcontroller (CPU) (Initial stop debug)
In the cyclic run mode, however, the following facilities that involve the programming of flash memory cannot be used.
When a core is in the following states, executing a program, referring to the CPU registers, and setting and deleting breakpoints are not possible.
When the core is in the following states, debugging is not possible. Only a subset of the debugging facilities, such as referring to states, is available.