Everything
2.11.4 Collect execution history only when the condition is met [IECUBE][Simulator]

The program execution history can be collected only when a condition is met.

By setting a Point Trace event, the execution history is collected as trace data only when an arbitrary variable or SFR is accessed with the specified type.

To use this function, follow the procedure described below.

 

2.11.4.1 Set a Point Trace event

2.11.4.2 Execute the program

2.11.4.3 Edit a Point Trace event

2.11.4.4 Delete a Point Trace event

Caution

[E1][E20][EZ Emulator][COM Port]
This function is not supported.