Everything
 

Scroll Range Settings dialog box


Set a range in which the vertical scroll bar of the Memory panel or Disassemble panel is scrolled.

When an appropriate range is set, the slider on the vertical scroll bar of the panel changes in size, so that dragging or the like operation with the mouse will be improved.

Caution

Even when, after a scroll range is set in this dialog box, the addresses represented by specified address expressions are altered by execution of a line assemble, etc., the scroll range is not corrected.

Remark

Movement in a panel window by the [Page Up], [Page Down], [Up] or [Down] key or a button at the end of the scroll bar, or by selection of a jump-related menu is possible, even outside the scroll range.

Figure A.47

Scroll Range Settings Dialog Box

 

This section describes the following.

[How to open]

-

On the Memory panel, select [View] and then click the button in the toolbar.

-

On the Memory panel, select [View] and then [Settings Scroll Range...] on the context menu.

-

On the Disassemble panel, select [View] and then click the button in the toolbar.

-

On the Disassemble panel, select [View] and then [Settings Scroll Range...] on the context menu.

[Description of each area]

(1)

[Start address] area

Specify the start address of a range to be scrolled.

Enter an address expression directly in the text box (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).

Note that if "All" in the drop-down list is selected, no scroll ranges are set (no limits to scroll range).

Remark

By pressing the [Ctrl] + [Space] keys in this text box, it is possible to complement a symbol name at the current caret position (see "2.21.2 Symbol name completion function").

(2)

[End address] area

Specify the end address of a range to be scrolled.

Enter an address expression directly in the text box (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).

However, this area disabled if "All" is specified in [Start address]].

Remark

By pressing the [Ctrl] + [Space] keys in this text box, it is possible to complement a symbol name at the current caret position (see "2.21.2 Symbol name completion function").

[Function buttons]

Button

Function

OK

Sets a specified scroll range in the panel concerned with it and moves the caret to the subject panel, with the start address appearing at the beginning of display.

Cancel

Nullifies settings and then closes this dialog box.

Help

Displays help for this dialog box.