Everything
2.16.1.3 Check the output result

The following figure shows how the value of the specified variable expression is output to the [Debug Tool] tab of the Output panel (see “Figure A.28 Output Result Format of Printf Event“).

Figure 2.170

Example of Output Result of Printf Event