Everything
2.5.2 An applied method of download

The files to download, as well as the download conditions applied at download time can be changed.

CS+ permits files in the following formats to be downloaded.

Table 2.2

Downloadable File Formats

File Format

Extension

Remark

Load module format

abs

 

Intel Hex format

-

Standard (offset address)

-

02 (segment address code)

-

04 (extension linear address code)

hex

03 (start segment address code) and 05 (start linear address code) are ignored.

Motorola S format

-

(S0, S1, S9-16 bits)

-

(S0, S2, S8-24 bits)

-

(S0, S3, S7-32 bits)

mot

 

Binary data format

bin

 

 

To change the download files, or set the download conditions applied at download time, use the Download Files dialog box shown below.

The Download Files dialog box is opened by clicking the [...] button that is displayed at the right edge in the column of the [Download files] property when you select it in the [Download] category on the Property panel's [Download File Settings] tab.

Figure 2.82

Opening the Download Files Dialog Box

Figure 2.83

An Applied Method of Download (Download Files Dialog Box)

 

Here, a method on how to set in the Download Files dialog box shown above is described, using the following cases as examples.

 

2.5.2.1 Changing the download conditions for load module files

2.5.2.2 Adding a download file (*.hex, *.mot, or *.bin)

2.5.2.3 Downloading multiple load module files

2.5.2.4 Performing source-level debug with hex format, Motorola S format, or binary data format files

2.5.2.5 Downloading files to external flash memory [E1] [E20]