Use the IOR panel shown below to display I/O register contents or change values.
Choose [IOR] from the [View] menu.
For details on how to read each area and details about their functionality, see the section where the IOR panel is described.

Following methods of operation are described here.
2.11.3.1 Searching I/O register
2.11.3.2 Putting the I/O registers in order
2.11.3.3 Changing the form in which values are displayed
2.11.3.4 Changing the contents of I/O registers
2.11.3.5 Displaying and changing I/O register contents during program execution