The Editor panel can be displayed in split form by using the vertical and horizontal splitter bars. The Editor panel can be split in up to two divisions vertically, and two divisions horizontally.
To remove the split, double-click any part of the splitter bar.
This function is disabled when the Mixed display mode is selected (setting to the mixed display mode removes the split).  |