Everything
2.2 Open Device Pin List Panel

Open the Device Pin List panel, where you enter information on the pins of the microcontroller.

To open the Device Pin List panel, double-click [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List] in the Project Tree panel.

Figure 2.1

Open Device Pin List Panel

 

Remark 1.

If an unsupported microcontroller is defined in the project for Pin Configurator, then "[Pin Configurator (Design Tool)] node" will hide under [Project name (Project)] in the Project Tree panel.

Remark 2.

The Device Pin List panel consists of three tabs. Selecting one of the tabs changes the order in which "information on each pin of the microcontroller" is displayed.

Information on each pin of the microcontroller is displayed in the order of pin number.

Information on each pin of the microcontroller is displayed in the order it was grouped into peripheral functions.

Information about the pins connected to external peripherals is displayed in order grouped at the external-peripheral component level.