This function writes to the memory.
[Specification format]
debugger.Memory.Write(address, value, memoryOption = MemoryOption.Byte)
|
[Argument(s)]
|
|
|
|
address
|
Specify the address to set.
|
|
value
|
Specify the value to set.
|
|
memoryOption
|
Specify the unit to set.
The units that can be specified are shown below.
|
|
|
|
|
MemoryOption.Byte
|
Byte unit (8 bits) (default)
|
|
MemoryOption.HalfWord
|
Half-word unit (16 bits) [RH850,RX,V850]
|
|
MemoryOption.Word
|
Word unit (RL78,78K: 16 bits, RH850,RX,V850: 32 bits)
|
[Return value]
If the memory was written to successfully: True
If there was an error when writing to the memory: False
[Detailed description]
- | This function sets the value at the address specified by address, according to memoryOption. |
- | When multiple values are to be written to consecutive addresses, using debugger.Memory.WriteRange reduces the overhead of processing for writing. |
[Example of use]
>>>debugger.Memory.Read(0x100)
0x10
>>>debugger.Memory.Write(0x100, 0xFF)
True
>>>debugger.Memory.Read(0x100)
0xFF
>>>debugger.Memory.Write(0x100, 0xFE, MemoryOption.HalfWord)
False
>>>
|