This tab shows the detailed information on subproject categorized by the following and the configuration can be changed.
[Description of each category]
The detailed information on files is displayed.
Displays the file name of the file to save the information on the subproject. |
||||
Displays the relative path of the subproject file to which subproject information is saved, from the location of the main project. This property is shown only when the subproject is selected in Project Tree panel. Note that if the relative path does not exist (such as the case that the main project and subproject are in the different drive), it is not displayed. |
||||
Displays the absolute path of the subproject file to save the information on them. |
||||
Select whether to save the subproject information to a subproject file using the absolute path. |
||||
The detailed information on a license is displayed and their configuration can be changed.
The detailed information on records is displayed and their configuration can be changed.
Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can use a text box directly enter the text. |
|||