Everything
2.11.1 Use rapid start

The rapid start function makes CS+ permanently resident, to accelerate the startup time.

You can enable or disable the rapid start in the [General - Startup and Exit] category in the Option dialog box, with option [Reduce startup time by enabling rapid startup] (Default: disabled).

 

When the rapid start is enabled, after login to Windows, CS+ is in the standby state, and the icon appears in the task tray.

Figure 2.108

Context Menu of Rapid Start Icon

(1)

Displaying the main window

To release CS+ from the standby state, and display the Main window, select [Start] in the context menu of the icon, or double-click the icon.

Click the button on the Main window to return CS+ to the standby state (an icon is displayed in the task tray during standby).

(2)

Exiting CS+

To exit CS+, select [Exit] in the context menu.