Panels support the auto-hide feature.
When the auto-hide feature is in use, unused panels are minimized on the edge of the frame, making it possible to display more information at one time.
To enable the auto-hide feature, click on the panel to hide to select it.
Right click on the panel's title bar, and select [Auto hide] or click on the panel's title bar 
.
When an auto-hidden panel loses the focus, a minimized icon and its panel name appear on the edge of the frame as a tab.
To display the auto-hidden panel, move the mouse cursor over the tab. The panel opens from the tab, and becomes available.
When the panel loses the focus again, the panel will be minimized as the tab.
To disable the auto-hide feature, click on the panel to hide to select it.
Right click on the panel's title bar, and select [Auto hide] or click on the panel's title bar 
.