Everything
D.1 Input Conventions

Below are input conventions for configuring information in the panels and dialog boxes provided by CS+.

(1)

Character sets

The following character sets are allowed for input.

Table D.1

List of Character Sets

Character Sets

Outline

ASCII

Single-byte numbers, letters, and punctuation

Shift-JIS

Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana

EUC-JP

Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji, and single-byte Katakana

UTF-8

Double-byte letters, numbers, punctuation, Hiragana, Katakana, and Kanji (including Chinese), and single-byte Katakana

(2)

Numbers

Numbers may be input in the following base formats.

Table D.2

List of Number Bases

Number Bases

Outline

Decimal number

Starts with 1 to 9, followed by a sequence of the digits 0 to 9, and 0

Hexadecimal number

Starts with 0x, followed by a sequence of the digits 0 to 9 and the letters a to f

(As for capital letter/small letter of the alphabet, it is pretermission.)