This tab shows the detailed information on a C source file categorized by the following and the configuration can be changed.
Note that this tab takes over the settings of the [Common Options] tab and [Compile Options] tab.
When the settings are changed from these tabs, the properties are displayed in boldface.
This tab is displayed only when [Yes] in the [Set individual compile option] property in the [Build] category from the [Build Settings] tab is selected.  | 
[Description of each category]
The detailed information on debug information is displayed and the configuration can be changed.
| 
 Select whether to generate the debug information. It is possible to perform source debugging with the debugger by outputting information for source debugging to the output file. This property corresponds to the -g option of the ccrl command.  | 
||||||
| 
 Select whether to enhance debug information at optimization. This property corresponds to the -g_line option of the ccrl command. This property is displayed in the following cases. 
  | 
||||||
The detailed information on the optimization is displayed and the configuration can be changed.
The detailed information on the optimization is displayed and the configuration can be changed.
| 
 Specify the maximum number of times to expand the loops such as "for" and "while". If 0 or 1 is specified, expansion is suppressed. If this is blank, the -Ounroll option is not added to the command line. In this case, a value in accordance with the selection of the [Level of optimization] property is used by the compiler. This property corresponds to the -Ounroll option of the ccrl command. This property is displayed only when [Perform the default optimization(No option specified)], [Code size precedence(-Osize)] or [Speed precedence(-Ospeed)] in the [Level of optimization] property is selected.  | 
||||||||||
| 
 Select whether to remove the static functions which are not called. This property corresponds to the -Odelete_static_func option of the ccrl command.  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Does not remove the unused static functions which are not called.  | 
||||||||||
| 
 Specify whether to perform inline expansion at the location calling functions. This property corresponds to the -Oinline_level option of the ccrl command. This property is displayed only when [Perform the default optimization(No option specified)], [Code size precedence(-Osize)] or [Speed precedence(-Ospeed)] in the [Level of optimization] property is selected.  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Performs inline expansion at the location calling the function for which #pragma inline is specified.  | 
||||||||||
| 
 Distinguishes the function that is the target of inline expansion automatically and expands it.  | 
||||||||||
| 
 Yes(Auto-detect without code size increase)(-Oinline_level=3)  | 
 Distinguishes the function that is the target of inline expansion automatically and expands it, while minimizing the increase in code size.  | 
|||||||||
| 
 Suppresses all inline expansion including the function for which "#pragma inline" is specified.  | 
||||||||||
| 
 Specify the maximum increasing rate (%) of the code size up to which inline expansion is performed. (Example: When "100" is specified, inline expansion will be applied until the code size increases by 100% (becomes twice the initial size).) This property corresponds to the -Oinline_size option of the ccrl command. This property is displayed only when [Yes(Auto-detect)(-Oinline=2)] in the [Perform inline expansion] property is selected, or when [To adjust the level of optimization(No option specified)] in the [Perform inline expansion] property and [Speed precedence(-Ospeed)] in the [Optimization Level] property are selected.  | 
||||||||||
| 
 Select whether to improve the program's execution performance by reordering instructions at the machine-language level. This property corresponds to the -Opipeline option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.03.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.03.00 or a later version of the CC-RL compiler has been installed.  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Use br instruction to call a function at the end of the function  | 
 Select whether to give precedence to using br instructions in the place of call instructions when the function ends with a function call. This property corresponds to the -Otail_call option of the ccrl command.  | 
|||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Gives precedence to using br instructions in the place of call instructions when the function ends with a function call. The code size can be reduced by removing the ret instruction.  | 
||||||||||
| 
 Uses call instructions when the function ends with a function call.  | 
||||||||||
| 
 Specify the level of inter-module optimization (such as function merging). This property corresponds to the -Ointermodule option of the ccrl command.  | 
||||||||||
| 
 Perform optimization considering type of data indicated by pointer  | 
 Select whether to perform optimization with consideration for the type of the data indicated by the pointer, based on the ANSI standard. This property corresponds to the -Oalias option of the ccrl command.  | 
|||||||||
| 
 Performs optimization with consideration for the type of the data indicated by the pointer. In general, this option improves the object performance, but the execution result may differ from the case when [No] is selected.  | 
||||||||||
| 
 Does not perform optimization with consideration for the type of the data indicated by the pointer.  | 
||||||||||
| 
 Select whether to create a subroutine for the same instruction sequence. This property corresponds to the -Osame_code option of the ccrl command. This property is displayed in the following cases. 
  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Does not create a subroutine for the same instruction sequence.  | 
||||||||||
| 
 Select whether to reduce the code size of the relative branch instructions. This property corresponds to the -Obranch_chaining option of the ccrl command. This property is displayed in the following cases. 
  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Rreduces the code size of the relative branch instructions..  | 
||||||||||
| 
 Does not reduce the code size of the relative branch instructions.  | 
||||||||||
| 
 Select whether to proceed with optimization through a change of the alignment conditions. This property corresponds to the -Oalign option of the ccrl command. This property is displayed in the following cases. 
 
 
  | 
||||||||||
| 
 Performs optimization according to the [Level of optimization] property.  | 
||||||||||
| 
 Performs optimization through a change of the alignment conditions.  | 
||||||||||
| 
 Does not perform optimization through a change of the alignment conditions.  | 
||||||||||
| 
 Outputs additional information for inter-module optimization  | 
 Select whether to output additional information for inter-module optimization. At linkage, inter-module optimization is applied to files for which this option has been specified. This property corresponds to the -goptimize option of the ccrl command.  | 
|||||||||
| 
 Outputs additional information for inter-module optimization.  | 
||||||||||
| 
 Does not outputs additional information for inter-module optimization.  | 
||||||||||
The detailed information on preprocessing is displayed and the configuration can be changed.
| 
 Specify the additional include paths during compiling. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The specified include path is searched with higher priority than the standard include file folder of CC-RL. The reference point of the path is the project folder. When this property is omitted, only the standard folder of CC-RL is searched. This property corresponds to the -I option of the ccrl command. The specified include path is displayed as the subproperty. Uppercase characters and lowercase characters are not distinguished for the include paths.  | 
||||||||
| 
 Edit by the Path Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box.  | 
||||||||
| 
 Select whether to compile using the include path specified in the [Additional include paths] property in the [Preprocess] category from the [Compile Options] tab of the build tool to be used. The include paths are added by the following procedure. 
 
 This property corresponds to the -I option of the ccrl command.  | 
||||||||
| 
 Compiles using the include path specified in the property of the build tool to be used.  | 
||||||||
| 
 Does not use the include path specified in the property of the build tool to be used.  | 
||||||||
| 
 Specify the file that is included at the top of the compilation unit. The following placeholders are supported. %ActiveProjectDir%: Replaces with the absolute path of the active project folder. %ActiveProjectName%: Replaces with the active project name. %BuildModeName%: Replaces with the build mode name. %MainProjectDir%: Replaces with the absolute path of the main project folder. %MainProjectName%: Replaces with the main project name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectDir%: Replaces with the absolute path of the project folder. %ProjectName%: Replaces with the project name. %TempDir%: Replaces with the absolute path of the temporary folder. %WinDir%: Replaces with the absolute path of the Windows system folder. The reference point of the path is the project folder. This property corresponds to the -preinclude option of the ccrl command. The specified include file name is displayed as the subproperty.  | 
||||||||
| 
 Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box.  | 
||||||||
| 
 Specify the name of the macro to be defined. Specify in the format of "macro name=defined value", with one macro name per line. The "=defined value" part can be omitted, and in this case, "1" is used as the defined value. This property corresponds to the -D option of the ccrl command.  | 
||||||||
| 
 Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box.  | 
||||||||
| 
 Specify the macro name to be undefined. Specify in the format of "macro name", with one macro name per line. This property corresponds to the -U option of the ccrl command.  | 
||||||||
| 
 Edit by the Text Edit dialog box which appears when clicking the [...] button. For the subproperty, you can enter directly in the text box.  | 
||||||||
| 
 Select whether to output the comments of the C source to the preprocessed file. This property corresponds to the -preprocess option of the ccrl command. This property is displayed only when [Yes(-P)] in the [Output preprocessed source file] property in the [Output File] category is selected.  | 
||||||||
| 
 Outputs the comments of the C source to the preprocessed file.  | 
||||||||
| 
 Does not output the comments of the C source to the preprocessed file.  | 
||||||||
| 
 Select whether to output the line number information of the C source to the preprocessed file. This property corresponds to the -preprocess option of the ccrl command. This property is displayed only when [Yes(-P)] in the [Output preprocessed source file] property in the [Output File] category is selected.  | 
||||||||
| 
 Outputs the line number information of the C source to the preprocessed file.  | 
||||||||
| 
 Does not output the line number information of the C source to the preprocessed file.  | 
||||||||
The detailed information on the quality improvement is displayed and the configuration can be changed.
| 
 Select whether to detect the stack smashing. This property is usable only in the Professional Edition. Detection of stack smashing is a feature for writing a value outside the valid stack area before entering a function and checking whether that value is rewritten before exiting the function. Upon detection, the user-defined __stack_chk_fail() function is called. See "CC-RL Compiler User's Manual" about the difference between [Yes(-stack_protector)] and [Yes(All)(-stack_protector_all)]. This property corresponds to the -stack_protector and -stack_protector_all options of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.02.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.02.00 or a later version of the CC-RL compiler has been installed.  | 
||||||
| 
 Specify the value to be embedded for detecting the stack smashing. This property is usable only in the Professional Edition. This property corresponds to the -stack_protector and -stack_protector_all options of the ccrl command. This property is displayed in the following cases. 
  | 
||||||
| 
 Select whether to output code for detecting illegal indirect function calls. Enable this facility to check the destination addresses of branches caused by each indirect function call. The output code will call the user-defined __control_flow_chk_fail() function in response to the detection of a problem. This property is usable only in the Professional Edition. This property corresponds to the -control_flow_integrity option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed.  | 
||||||
| 
 Does not output code for detecting illegal indirect function calls.  | 
||||||
The detailed information on C language is displayed and the configuration can be changed.
| 
 Select the standard of C language. This property corresponds to the -lang option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed. 
  | 
||||||
| 
 Compilation will proceed in compliance with the C90 standard.  | 
||||||
| 
 Compilation will proceed in compliance with the C99 standard.  | 
||||||
| 
 Select whether to process as making C source program comply strictly with the ANSI standard and output an error or warning for a specification that violates the standard. This property corresponds to the -ansi option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.05.00 or an earlier version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.05.00 or an earlier version of the CC-RL compiler has been installed.  | 
||||||
| 
 Processes as making C source program comply strictly with the ANSI standard and outputs an error or warning for a specification that violates the standard.  | 
||||||
| 
 Compatibility with the conventional C language specifications is conferred and processing continues after warning is output.  | 
||||||
| 
 Select whether to process as making C source program comply strictly with the C90 or C99 standard and output an error or warning for a specification that violates the standard. This property corresponds to the -strict_std option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed.  | 
||||||
| 
 Processes as making C source program comply strictly with the C90 or C99 standard and outputs an error or warning for a specification that violates the standard.  | 
||||||
| 
 Compatibility with the conventional C language specifications is conferred and processing continues after warning is output.  | 
||||||
| 
 Select whether to generate an error when using a function whose prototype declaration was not made in advance or a function without a prototype declaration. This property corresponds to the -refs_without_declaration option of the ccrl command.  | 
||||||
| 
 Select whether to increase the maximum variable size from 0x7fff to 0xffff. This property corresponds to the -large_variable option of the ccrl command.  | 
||||||
| 
 Select whether to allow the nest use of comments ("/**/"). This property corresponds to the -nest_comment option of the ccrl command.  | 
||||||
The detailed information on character encoding is displayed and the configuration can be changed.
The detailed information on output code is displayed and the configuration can be changed.
| 
 Select whether to handle all external variables and variables specified with #pragma address as if they are volatile qualified. This property corresponds to the -volatile option of the ccrl command.  | 
||||
| 
 Handles all external variables and variables specified with #pragma address as if they are volatile qualified.  | 
||||
| 
 Optimizes external variables that are not volatile qualified.  | 
||||
| 
 Select the code output mode for switch statements in programs. This property corresponds to the -switch option of the ccrl command.  | 
||||
| 
 Outputs the switch statements in the same format as the if-else statement along a string of case statements in programs. Select this item if the case statements are written in the order of frequency or if only a few labels are used. Because the case statements are compared starting from the top, unnecessary comparison can be reduced and the execution speed can be increased if the case statement that most often matches is written first.  | 
||||
| 
 Outputs the code in the binary search format for switch statements in programs. Searches for a matching case statement by using a binary search algorithm. If this item is selected when many labels are used, any case statement can be found at almost the same speed.  | 
||||
| 
 Outputs the code in the table jump format (absolute branch) for switch statements in programs. References a table indexed on the values in the case statements, and selects and processes case labels from the switch statement values. The code will branch to all the case statements with about the same speed. However, if case values are not used in succession, an unnecessary area will be created.  | 
||||
| 
 Outputs the code in the table jump format (relative branch) for switch statements in programs. References a table indexed on the values in the case statements, and selects and processes case labels from the switch statement values. The code will branch to all the case statements with about the same speed. However, if case values are not used in succession, an unnecessary area will be created.  | 
||||
| 
 Select whether to perform indirect referencing in 1-byte units. This property corresponds to the -unaligned_pointer_for_ca78k0r option of the ccrl command. When [Yes(-unaligned_pointer_for_ca78k0r)] is selected, if there is a possibility that a pointer to a type having a 2-byte alignment condition without volatile keyword points to an odd address, code for indirect reference in 1-byte units are generated. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed.  | 
||||
| 
 Select whether to output a C source program as a comment to the assembly source file to be output. This property corresponds to the -pass_source option of the ccrl command. This property is displayed only when [Yes(-asm_path)] in the [Output assembly source file] property in the [Output File] category is selected or when [Yes(-asmopt=-prn_path)] in the [Output assemble list file] property in the [Assemble List] category is selected.  | 
||||
| 
 Outputs a C source program as a comment to the assembly source file.  | 
||||
| 
 Does not output a C source program as a comment to the assembly source file.  | 
||||
| 
 When the same string literals exist in the source file, specify whether to merge them and allocate to the one area. This property corresponds to the -merge_string option of the ccrl command.  | 
||||
| 
 Merges the same string literals exist in the source file and allocates to the one area.  | 
||||
| 
 Each allocates the same string literals exist in the source file to separate areas.  | 
||||
| 
 Allocate uninitialized variables in sections according to number of alignments  | 
 Select whether to allocate the uninitialized variables to sections in accord with their alignment sizes. This property corresponds to the -stuff option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.10.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.10.00 or a later version of the CC-RL compiler has been installed.  | 
|||
| 
 Allocates the uninitialized variables to sections in accord with their alignment sizes.  | 
||||
| 
 Does not allocate the uninitialized variables to sections in accord with their alignment sizes.  | 
||||
| 
 Allocate initialized variables in sections according to number of alignments  | 
 Select whether to allocate the initialized variables to sections in accord with their alignment sizes. This property corresponds to the -stuff option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.10.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.10.00 or a later version of the CC-RL compiler has been installed.  | 
|||
| 
 Allocates the initialized variables to sections in accord with their alignment sizes.  | 
||||
| 
 Does not allocate the initialized variables to sections in accord with their alignment sizes.  | 
||||
| 
 Allocate const qualified variables in sections according to number of alignments  | 
 Select whether to allocate the const qualified variables to sections in accord with their alignment sizes. This property corresponds to the -stuff option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.10.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.10.00 or a later version of the CC-RL compiler has been installed.  | 
|||
| 
 Allocates the const qualified variables to sections in accord with their alignment sizes.  | 
||||
| 
 Does not allocate the const qualified variables to sections in accord with their alignment sizes.  | 
||||
The detailed information on output files is displayed and the configuration can be changed.
The detailed information on the assemble list is displayed and the configuration can be changed.
The detailed information on the MISRA-C rule check are displayed and the configuration can be changed.
20XX in the following table corresponds to 2012 or 2004 in particular.
| 
 Select the MISRA-C specification. This property is usable only in the Professional Edition. This property is displayed when [Always latest version which was installed] or V1.02.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.02.00 or a later version of the CC-RL compiler has been installed.  | 
||||||||||||
| 
 Settings for MISRA-C 2012 are made in the subsequent properties.  | 
||||||||||||
| 
 Settings for MISRA-C 2004 are made in the subsequent properties.  | 
||||||||||||
| 
 Select the MISRA-C rules to be applied. This property is usable only in the Professional Edition. This property corresponds to the -misra20XX option of the ccrl command.  | 
||||||||||||
| 
 Checks the source code against all of the rules which are supported.  | 
||||||||||||
| 
 Checks the source code against the rules with the specified numbers among the rules which are supported.  | 
||||||||||||
| 
 Checks the source code against the rules that do not match the specified numbers among the rules which are supported.  | 
||||||||||||
| 
 Apply rules that are classified as "required"(-misra20XX=required)  | 
 Checks the source code against the rules of the "required" type.  | 
|||||||||||
| 
 Apply rules that are classified as "required" and specified rule number(-misra20XX=required_add)  | 
 Checks the source code against the rules of the "required" type and the rules with the specified numbers among the rules which are supported.  | 
|||||||||||
| 
 Ignore specified rule number from rules that are classified as "required"(-misra20XX=required_remove)  | 
 Checks the source code against the rules of the "required" type except for the rules with the specified numbers among the rules which are supported.  | 
|||||||||||
| 
 Apply rules that are described in the specified file(-misra20XX=<file name>)  | 
 Checks the source code against the rules with the numbers described in specified file among the rules which are supported.  | 
|||||||||||
| 
 Specify the rule number description file (MISRA-C rule file). This property is usable only in the Professional Edition. When misra2012 is selected, the CC-RL compiler always checks the code against rule numbers 13.6, 17.3, and 17.4 (as well as 9.1 if the compiler is V1.04.00 or later, 12.5 and 21.13 if the compiler is V1.05.00 or later, and 17.6 if the compiler is V1.06.00 or later) regardless of which rule numbers have been specified through the properties setting. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectName%: Replaces with the project name. This property corresponds to the -misra20XX option of the ccrl command. This property is displayed only when [Apply rules that are described in the specified file(-misra20XX=<file name>)] in the [Apply rule] property is selected.  | 
||||||||||||
| 
 Directly enter in the text box or edit by the Specify MISRA-C Rule File dialog box which appears when clicking the [...] button.  | 
||||||||||||
| 
 Specify the rule number to be checked. This property is usable only in the Professional Edition. When misra2012 is selected, the CC-RL compiler always checks the code against rule numbers 13.6, 17.3, and 17.4 (as well as 9.1 if the compiler is V1.04.00 or later, 12.5 and 21.13 if the compiler is V1.05.00 or later, and 17.6 if the compiler is V1.06.00 or later) regardless of which rule numbers have been specified through the properties setting. Specify at least one rule number in decimal. This property corresponds to the -misra20XX option of the ccrl command. This property is displayed only when [Apply specified rule number(-misra20XX=apply)] in the [Apply rule] property is selected.  | 
||||||||||||
| 
 Directly enter in the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button.  | 
||||||||||||
| 
 Specify the rule number to be excluded from the check. This property is usable only in the Professional Edition. When misra2012 is selected, the CC-RL compiler always checks the code against rule numbers 13.6, 17.3, and 17.4 (as well as 9.1 if the compiler is V1.04.00 or later, 12.5 and 21.13 if the compiler is V1.05.00 or later, and 17.6 if the compiler is V1.06.00 or later) regardless of which rule numbers have been specified through the properties setting. Specify at least one rule number in decimal. This property corresponds to the -misra20XX option of the ccrl command. This property is displayed only when [Ignore specified rule number(-misra20XX=ignore)] in the [Apply rule] property is selected.  | 
||||||||||||
| 
 Directly enter in the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button.  | 
||||||||||||
| 
 Specify the rule number to be checked besides the required rules. This property is usable only in the Professional Edition. When misra2012 is selected, the CC-RL compiler always checks the code against rule numbers 13.6, 17.3, and 17.4 (as well as 9.1 if the compiler is V1.04.00 or later, 12.5 and 21.13 if the compiler is V1.05.00 or later, and 17.6 if the compiler is V1.06.00 or later) regardless of which rule numbers have been specified through the properties setting. Specify at least one rule number in decimal. This property corresponds to the -misra20XX option of the ccrl command. This property is displayed only when [Apply rules that are classified as "required" and specified rule number(-misra20XX=required_add)] in the [Apply rule] property is selected.  | 
||||||||||||
| 
 Directly enter in the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button.  | 
||||||||||||
| 
 Specify the required rule number to be excluded from the check. This property is usable only in the Professional Edition. When misra2012 is selected, the CC-RL compiler always checks the code against rule numbers 13.6, 17.3, and 17.4 (as well as 9.1 if the compiler is V1.04.00 or later, 12.5 and 21.13 if the compiler is V1.05.00 or later, and 17.6 if the compiler is V1.06.00 or later) regardless of which rule numbers have been specified through the properties setting. Specify at least one rule number in decimal. This property corresponds to the -misra20XX option of the ccrl command. This property is displayed only when [Ignore specified rule number from rules that are classified as "required"(-misra20XX=required_remove)] in the [Apply rule] property is selected.  | 
||||||||||||
| 
 Directly enter in the text box or edit by the Specify Rule Number dialog box which appears when clicking the [...] button.  | 
||||||||||||
| 
 Specify files that will not be checked against the MISRA-C rules. This property is usable only in the Professional Edition. The following placeholders are supported. %BuildModeName%: Replaces with the build mode name. %MicomToolPath%: Replaces with the absolute path of the install folder of this product. %ProjectName%: Replaces with the project name. This property corresponds to the -ignore_files_misra option of the ccrl command. This property is displayed only in the following cases. 
 
 
 
  | 
||||||||||||
| 
 Edit by the Path Edit dialog box which appears when clicking the [...] button. -> Edit by the Add Excluding File dialog box which appears when clicking the [Browse...] button. For the subproperty, you can enter directly in the text box.  | 
||||||||||||
| 
 Output message of the enhanced key word and extended specifications  | 
 Select whether to output the message of the enhanced key word and extended specifications. This property is usable only in the Professional Edition. This property corresponds to the -check_language_extention option of the ccrl command. This property is displayed only in the following cases. 
 
 
 
  | 
|||||||||||
| 
 Enables MISRA-C rule check and outputs messages when the rule check is partially suppressed by the unique language specifications extended from the C language standard.  | 
||||||||||||
| 
 Disables MISRA-C rule check is disabled, which are partially suppressed by the extended language specifications.  | 
||||||||||||
| 
 Select whether to enable checking that spans files. This property is usable only in the Professional Edition. This property corresponds to the -misra_intermodule option of the ccrl command. This property is displayed only in the following cases. 
  | 
||||||||||||
The detailed information on the error output is displayed and the configuration can be changed.
| 
 Select whether to output the error message file. This property corresponds to the -error_file option of the ccrl command. Error messages are displayed on the Output panel regardless of this property's. This property is displayed only when [No] in the [Build in parallel] property in the [Build Method] category from the [Common Options] tab is selected  | 
||||
| 
 Specify the folder which the error message file is output. If a relative path is specified, the reference point of the path is the main project or subproject folder. If an absolute path is specified, the reference point of the path is the main project or subproject folder (unless the drives are different). The following placeholder is supported. %BuildModeName%: Replaces with the build mode name. If this is blank, it is assumed that the project folder has been specified. This property corresponds to the -error_file option of the ccrl command. This property is displayed only when [Yes(-error_file)] in the [Output error message file] property is selected.  | 
||||
| 
 Directly enter in the text box or edit by the Browse For Folder dialog box which appears when clicking the [...] button.  | 
||||
| 
 Specify the error message file name. The extension can be freely specified. The following placeholders are supported. %ActiveProjectName%: Replaces with the active project name. %MainProjectName%: Replaces with the main project name. %ProjectName%: Replaces with the project name. If this is blank, it is assumed that "%ProjectName%.err" has been specified. This property corresponds to the -error_file option of the ccrl command. This property is displayed only when [Yes(-error_file)] in the [Output error message file] property is selected.  | 
||||
The detailed information on warning messages is displayed and the configuration can be changed.
The detailed information on messages is displayed and the configuration can be changed.
| 
 Select whether to change the type of warning messages to error. This property corresponds to the -change_message option of the ccrl command. This property is displayed when [Always latest version which was installed] or V1.06.00 or a later version is selected for the [Using compiler package version] property under the [Version Select] category on the [Common Options] tab in an environment where V1.06.00 or a later version of the CC-RL compiler has been installed.  | 
||||||
| 
 Yes(Specify message number)(-change_message=error=<Message number>)  | 
 Specifies the number of warning message of which type is to be changed to error.  | 
|||||
| 
 Specify the number of the warning message. If multiple message numbers are specified, delimit them with "," (comma) (example: 23028,23086). Also, a range of message numbers can be specified using "-" (hyphen) (example:23028-23086). This property corresponds to the -change_message option of the ccrl command. This property is displayed only in the following cases. 
  | 
||||||
| 
 Directly enter in the text box or edit by the Character String Input dialog box which appears when clicking the [...] button.  | 
||||||
Other detailed information on compilation is displayed and the configuration can be changed.