If the C source program falls under any of the following items, it may not be possible for the CC-RL to correctly compile the converted C source program.
| 
 When a keyword cannot be detected because a ## operator is being used  | 
||||
| 
 When '?' is included in the section name for #pragma section  | 
||||
| 
 When a section name that does not exist in the CC-RL is specified for the section name of #pragma section  | 
 Warning W0523037 is output and the #pragma directive is ignored. There is a possibility that section allocation will fail and operation is not as expected.  | 
|||
| 
 When "/*" is included in an assembly-language comment (description after ";") within the range of #asm-#endasm  | 
 A C-language comment ("/*") is given priority over an assembly-language comment (";") and the range of the comment is invalid.  | 
|||
| 
 When a label is included in __asm( ) or the assembly-language code within #asm-#endasm  | 
 [Restrictions] of #pragma inline_asm in the CC-RL user's manual  | 
|||
| 
 When a 78K0-specific instruction or an instruction whose operation differs from that of RL78 is used in __asm() or the assembly-language code of #asm-#endasm  | 
 No message is output and instructions are output without change to the #pragma inline_asm function.  | 
 When a 78K0-specific instruction is used, an assembly error will occur. When an instruction whose operation differs from that of RL78 is used, operation may not be as expected.  | 
||
| 
 When there is #pragma interrupt and a description of the __interrupt keyword for the same function in a file  | 
 There will be duplicate #pragma directives and error E0523006 will occur.  | 
|||
| 
 When parameters in function declarations __interrupt, __interrupt_brk, and __rtos_interrupt are omitted  | 
 A #pragma directive is output and function declarations are output without change.  | 
 Error E0523008 will occur since there is no void type specification.  | 
||
| 
 When a macro or typedef is used in code for obtaining a type name, function name, variable name, etc.  | 
 A message is output and the program is output without being converted.  | 
|||
| 
 When there is #pragma rtos_interrupt and a description of the __rtos_interrupt keyword for the same function in a file  | 
 There will be duplicate #pragma directives and error E0523006 will occur.  | 
|||
| 
 When the same address is specified for different variables in __directmap  | 
 Absolute Address Allocation Specification [Restrictions] of #pragma address in the CC-RL user's manual  |