12-bit interval timer
Below is a list of API functions output by the Code Generator for 12-bit interval timer use.
Table 3.16 API Functions: [12-Bit Interval Timer]
|
API Function Name |
Function |
|
Performs initialization necessary to control the 12-bit interval timer. | |
|
Performs user-defined initialization relating to the 12-bit interval timer. | |
|
Performs processing in response to the 12-bit interval timer interrupt INTIT. | |
|
Starts the count of the 12-bit interval timer. | |
|
Ends the count of the 12-bit interval timer. | |
|
Reset the 12-bit interval timer. | |
|
Halts the clock supplied to the 12-bit interval timer. |