R_TAUm_Channeln_Lower8bits_Stop
 
Ends the count (lower 8-bit) for 
channel n.
Remark         
This API function can only be called when the timer array unit is used as a 
8-bit timer.
 
[Syntax]
void       
R_TAUm_Channeln_Lower8bits_Stop ( void );
 
Remark         
m is the unit number, and n is the channel number.
 
[Argument(s)]
None.
 
[Return 
value]
None.