Changes the operating power control mode of the MCU.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_lpc.h"
MD_STATUS R_LPC_ChangeOperatingPowerControl ( operating_mode_t mode );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       I  | 
    
       operating_mode_t mode;  | 
    
       Operating power control mode type HIGH_SPEED : High-speed operating mode MIDDLE_SPEED : Middle-speed operating mode LOW_SPEED : Low-speed operating mode  | 
[Return value]
| 
       Macro  | 
    
       Description  | 
| 
       MD_OK  | 
    
       Normal completion  | 
| 
       MD_ERROR1  | 
    
       Change to the low-speed operating mode ended abnormally.  | 
| 
       MD_ERROR2  | 
    
       Change to the middle-speed operating mode is ended abnormally.  | 
| 
       MD_ARGERROR  | 
    
       Invalid argument mode specification  |