Performs processing in response to the RSPI error interrupts.
Remark This API function is called as the r_rspin_error_interrupt callback routine.
[Syntax]
static void r_rspin_callback_error ( uint8_t err_type );
Remark n is the channel number.
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       uint8_t err_type;  | 
    
       Source of the RSPI error interrupt (x is undefined) xxxx00x1B : Overrun error detection xxxx01x0B : Mode fault error detection xxxx10x0B : Parity error detection  | 
[Return value]
None.