frsm_tsk
ifrsm_tsk
ER frsm_tsk (ID tskid);
ER ifrsm_tsk (ID tskid);
 These service calls cancel all of the suspend requests issued for the task specified by parameter tskid (by setting the suspend request counter to 0). As a result, the target task moves from the SUSPENDED state to the READY state, or from the WAITING-SUSPENDED state to the WAITING state.
 Note 1	 These service calls do not perform queuing of forced cancelation requests. If the target task is neither in the SUSPENDED state nor WAITING-SUSPENDED state, "E_OBJ" is returned.
 Note 2	 The RI600V4 does not support queuing of suspend request. Therefore, the behavior of these service calls are same as rsm_tsk and irsm_tsk.