fsnd_dtq
ifsnd_dtq
ER fsnd_dtq (ID dtqid, VP_INT data);
ER ifsnd_dtq (ID dtqid, VP_INT data);
 These service calls process as follows according to the situation of the data queue specified by the parameter dtqid.
 -	 There is a task in the reception wait queue.
This service call transfers the data specified by parameter data to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
This service call transfers the data specified by parameter data to the task in the top of the reception wait queue. As a result, the task is unlinked from the reception wait queue and moves from the WAITING state (data reception wait state) to the READY state, or from the WAITING-SUSPENDED state to the SUSPENDED state.
 -	 There is no task neither in the reception wait queue and transmission wait queue.
This service call stores the data specified by parameter data to the data queue.
If there is no available space in the data queue, this service call deletes the oldest data in the data queue before storing the data specified by data to the data queue.
This service call stores the data specified by parameter data to the data queue.
If there is no available space in the data queue, this service call deletes the oldest data in the data queue before storing the data specified by data to the data queue.