-   
 
   Main window
  
    -   
  
 
 This is the first window to be open when the CS+ is launched.
 
 This window is used to control the user program execution and open panels for the build process.
 
 This window can be opened as follows:
 
 -	 Select Windows [start] -> [All programs] -> [Renesas Electronics CS+] -> [CS+]
 
 Displays the menus relate to realtime OS.
 
 Contents of each menu can be customized in the User Setting dialog box.
 
 
  
  
    | 
 | 
    
 The [View] menu shows the cascading menu to start the tools of realtime OS.
  
 | 
  
  
    | 
 | 
    
 | 
    
 Opens the Realtime OS Resource Information panel.
  
 Note that this menu is disabled when the debug tool is not connected.
  
 | 
  
  
    | 
 | 
    
 Opens the Task Analyzer window.
  
 Note that this menu is disabled when the debug tool is not connected.
  
 | 
  
 
 Displays the buttons relate to realtime OS.
 
 Buttons on the toolbar can be customized in the User Setting dialog box. You can also create a new toolbar in the same dialog box.
 
 
  
  
    | 
 | 
    
 Opens the Realtime OS Resource Information panel.
  
 Note that this button is disabled when the debug tool is not connected.
 
 | 
  
 
 
  
  
    | 
 | 
    
 Opens the Realtime OS Task Analyzer panel.
  
 Note that this button is disabled when the debug tool is not connected.
 
 | 
  
 
 The following panels are displayed in this area.
 
 See the each panel section for details of the contents of the display.
 
 Note See "CS+ Integrated Development User's Manual: RL78 Build" for details about the Output panel.