17.4.3 FPSR register information
The initial FPSR register value specified in this item is loaded in the FPSR register at the initial activation of a processing program (such as a task, a cyclic handler, or an interrupt handler).
1 ) Initial FPSR register value: fpsr
Specifies the initial value to be loaded in the FPSR at initial activation of a processing program.
A value from 0x0 to 0xffffffff can be specified for fpsr.
Note that operation is not guaranteed if a value outside the range allowed by hardware is specified. See the hardware manual for the specific values.
Specifies the initial value to be loaded in the FPSR at initial activation of a processing program.
A value from 0x0 to 0xffffffff can be specified for fpsr.
Note that operation is not guaranteed if a value outside the range allowed by hardware is specified. See the hardware manual for the specific values.