|
-LIB_REName [V2.01.00 or later]
|
This option changes a symbol name or section name that was input from a library.
[Specification format]
-lib_rename=name1=name2[, ...]
-lib_rename=file(name1=name2[, ...])
-lib_rename="file|module[|module ...](name1=name2[, ...])"
|
- | Interpretation when omitted |
None
[Detailed description]
- | This option changes the name of an external symbol or section included in a module within the library that was specified by the -library option. |
- | Specify the symbol name or section name to be changed as name1. Specify the symbol name or section name after the change as name2. |
- | When you specify a C variable name, add prefix "_" to the definition name in the program. |
- | If the specified name matches both section and symbol names, the symbol name is changed. |
- | If there are two or more files or modules with the same name, the priority depends on the input order. |
- | If this option is specified more than once, all specifications will be valid. |
- | An error will occur in any of the following cases. |
- | When the specified name, file, or module cannot be found |
- | When the parameter is omitted |
- | When this option is specified together with the -form={object,library}, -extract, or -strip option |
[Remark]
- | When the -form={absolute|hexadecimal|stype|binary} option is specified, the -show=struct option cannot be specified together. |
- | The section name of the input library cannot be changed. |
- | Correct operation is not guaranteed if this option is used in combination with the compiler option -Xmerge_files. |
[Example of use]
- | To change "_sym1" in b.lib and c.lib to "_data", describe as: |
>rlink a.obj -lib=b.lib,c.lib -lib_rename=(_sym1=_data)
|
- | To change "_sym1" in all modules in b.lib to "_data", describe as: |
>rlink a.obj -lib=b.lib,c.lib -lib_rename=b.lib(_sym1=_data)
|
- | To change "_sym1" in modules m1 and m2 in b.lib to "_data", describe as: |
>rlink a.obj -lib=b.lib,c.lib -lib_rename="b.lib|m1|m2(_sym1=_data)"
|