The CC-RH provides the following libraries.
|
Functions with variable arguments Character conversion functions Character classification functions Peripheral device initialization function RAM section initialization function Checks for indirect function calls function) (Mathematical functions (Double-precision and single-precision)) |
When -Xfloat=fpu, -Xdbl_size=8, and -Xround=nearest are specified |
|
|
When -Xfloat=soft, -Xdbl_size=8, and -Xround=nearest are specified |
||
|
When -Xfloat=fpu, -Xdbl_size=4, and -Xround=nearest are specified |
||
|
When -Xfloat=soft, -Xdbl_size=4, and -Xround=nearest are specified |
||
|
When -Xfloat=fpu, -Xdbl_size=8, and -Xround=zero are specified |
||
|
When -Xfloat=fpu, -Xdbl_size=4, and -Xround=zero are specified |
||
|
Functions with variable arguments Character conversion functions Character classification functions Peripheral device initialization function |
Can always be used (for backward compatibility with V1.01.00 or earlier) |
|
|
Mathematical library using FPU (Mathematical functions (Double-precision)) |
When -Xfloat=fpu is specified (for backward compatibility with V1.01.00 or earlier) |
|
|
Mathematical library using FPU (Mathematical functions (Single-precision)) |
||
|
Mathematical library not using FPU (Mathematical functions (Double-precision)) |
When -Xfloat=soft is specified (for backward compatibility with V1.01.00 or earlier) |
|
|
Mathematical library not using FPU (Mathematical functions (Single-precision)) |
|
Functions with variable arguments Character conversion functions Character classification functions Peripheral device initialization function |
||
|
Mathematical library using FPU (Mathematical functions (Double-precision)) |
||
|
Mathematical library using FPU (Mathematical functions (Single-precision)) |
||
|
Mathematical library not using FPU (Mathematical functions (Double-precision)) |
||
|
Mathematical library not using FPU (Mathematical functions (Single-precision)) |
||
When the standard library or mathematical library is used in an application, include the related header files to use the library function. |
Refer these libraries using the optimizing linker option (-l).
However, it is not necessary to refer the libraries if only "program diagnosis function", "function with a variable arguments", "character conversion functions" and "character classification functions" are used.
The operation runtime function is a routine that is automatically called by the CC-RH when a floating-point operation or integer operation is performed. |
Unlike the other library functions, the "operation runtime function" is not described in the C source or assembler source.
Each rh***.lib library includes the contents of libc.lib, libm.lib, and libmf.lib (but does not include libmalloc.lib, libsetjmp.lib). When specifying an rh***.lib library, do not specify libc.lib, libm.lib, or libmf.lib together. In addition, only one of the rh***.lib libraries should be specified. Otherwise, correct operation is not guaranteed. |