< Assembler Command Options / Object Options >
When a Motorola S-record file (<name>.mot) or Hex file (<name>.hex) is output, this option blocks spaces created by .OFFSET directives in the assembly language being filled with output data.  | 
When using this option, specify it when using the ccrx or asrx command to create an object file (<name>.obj) as well as when using the rlink command to create a Motorola S-record file or Hex file.  | 
When this option is used, symbols in the format shown below*1 will be added for each .OFFSET directive.  | 
*1) Since symbols in this format are reserved, they cannot be directly included in your source code.