2.19.4.2
Edit access-related events
The address condition, data condition and pass count condition [Simulator] for access-related events you have set can be edited.
Perform this operation in the Detail dialog box (for access events) that is opened by selecting [Edit Condition...] from the context menu after moving the caret to an access-related eventNote you want to edit on the Events panel.
Note | An access-related event refers to any one of the following events in the Events panel. |
- | Hardware Break event (access type) |
- | Access-related event as start and end condition in detailed information on Trace event |
- | Access-related event in detailed information on Point Trace event |
- | Access-related event as start and end condition in detailed information on Performance Measurement event |
For the access-related events that were set according to the descriptions in 2.11.5.1 Set a break event (access type), 2.14.3.1 Set a Trace event, 2.14.4.1 Set a Point Trace event, and 2.16.1.1 Set a Performance Measurement event the initial values of the address, data, and pass count conditions are listed below.
Table 2.25 | Initial Values of Address Conditions |
|
|
|
|
Compare condition
|
[Full-spec emulator][E1][E20]
RH850G3M, RH850G3K, RH850G3MH, RH850G3KH:
Specified address (==)
RH850G4MH:
When a value for comparison has been specified:
Inside the range (<=Addresses<=)
When a value for comparison has not been specified:
Specified address (==)
GTM:
Inside the range (<=Addresses<=)
[Simulator]
Specified address (==)
|
[Full-spec emulator][E1][E20]
Inside the range (<=Addresses<=)
[Simulator]
Specified address (==)
|
Address
|
Address at the time of setting the event
|
Start address
|
Address at the time of setting the event
|
End address
|
Address at the time of setting the event
|
Use the address mask
|
No
|
Mask value
|
0xFFFFFFFF
|
Table 2.26 | Initial Values of Data Conditions |
Item
|
Initial Value
|
Access type
|
Access type at the time of setting the event
|
Access size
|
Variable or I/O register size at the time of setting the event
|
Compare condition
|
When a value for comparison has been specified : Specified value (==)
When a value for comparison has not been specified : No conditions
|
Data
|
Data at the time of setting the event
|
Lower data
|
Data at the time of setting the event
|
Upper data
|
Data at the time of setting the event
|
Use the data mask
|
No
|
Mask value
|
0xFFFFFFFF
|
Table 2.27 | Initial Values of Pass count Conditions |
Item
|
Initial Value
|
Pass count [Simulator]
|
1
|