This panel is central to the functionality of the solution for measurement of CAN bus reception processing times.
See "2.25 Measuring CAN Bus Reception Processing Times [E2]" for details on the solution for measurement of CAN bus reception processing times.
This section describes the following.
A warning will appear in this area when the current settings for measuring CAN bus reception processing times do not satisfy the conditions required prior to connection of the debug tool. This area is hidden when there is no warning to be reported.
This area displays the conditions for measuring CAN bus reception processing times.
Note that you can only view the current settings in this area. To make settings, use the Measurement Condition Setting dialog box [E2] opened by selecting [Set Condition] -> [Set Condition n...].
You can select up to two conditions. |
This area is used to make general settings that will apply to all measurements, regardless of conditions 1 and 2.
Select the operation of the debugger after the recording memory of the emulator becomes full during measurement from the following drop-down list.
Select this check box if you have built a program with the inclusion of automatically inserted dbtag instructions and wish to apply this build option to the given property of the build tool.
This check box is selectable when V1.06.00 or later of the CC-RH compiler is selected for the active project. |
This area displays the results of measuring CAN bus reception processing times (minimum time, maximum time, average time, and number of measurement).
|
Starts measuring the CAN bus reception processing time. When V1.06.00 or later of the CC-RH compiler is selected for the active project, prior to measurement, rebuilding to insert dbtag instructions and downloading of the result proceed. |
||
|
Starts measuring the CAN bus reception processing time. Rebuilding to insert dbtag instructions and downloading of the result do not proceed. Note that this button appears when V1.06.00 or later of the CC-RH compiler is selected for the active project. |
||
|
Has the same functionality as the same button on the Debug toolbar in the Main window. |
||
|
The following cascade menus are displayed to set conditions for measurement of the CAN bus reception processing time. |
||
|
Opens the Measurement Condition Setting dialog box [E2] to make settings for measurement condition 1. |
||
|
Opens the Measurement Condition Setting dialog box [E2] to make settings for measurement condition 2. |
||
|
The following cascade menus are displayed to delete the delete the condition for measurement of the CAN bus reception processing time. |
||
|
Clears the log of measurement results of the CAN bus reception processing time. |
||
|
Opens the Save File dialog box to save measurement results of the CAN bus reception processing time to a CSV file or Microsoft Office Excel book. |
||
|
The following cascade menus are displayed to set conditions for measurement of the CAN bus reception processing time. |
||
|
Opens the Measurement Condition Setting dialog box [E2] to make settings for measurement condition 1. |
||
|
Opens the Measurement Condition Setting dialog box [E2] to make settings for measurement condition 2. |
||
|
The following cascade menus are displayed to delete the delete the condition for measurement of the CAN bus reception processing time. |
||
|
Clears the log of measurement results of the CAN bus reception processing time. |
||