Everything
2.11.1 Configure the trace operation

When the trace function starts, trace data which has recorded in it an execution history of the currently executed program is collected in trace memory (when program execution stops, the trace function also automatically stops).

Before the trace function can be used, it is necessary to make settings relating to the operation of a trace.

Note that the method on how to set differs depending on the debug tool used.

 

2.11.1.1 [IECUBE]

2.11.1.2 [E1]/[E20]/[EZ Emulator]/[COM Port]

2.11.1.3 [Simulator]