Everything
2.15.7.2 Event types that can be set and deleted during execution

Types of events that can be set or removed during execution of the program or during execution of the tracer/timer are described below.

The meaning of each mark in the table below is as follows:

 

Possible

 

Possible, if the program execution is allowed to pause for events
(Property panel >> [Debug Tool Settings] tab >> [Set Event While Running] category >> [Set event by stopping execution momentarily] property >> [Yes])

 

Impossible while tracer or timer is executing

-

Impossible, or not supported

Table 2.21

Event Types That Can be Set and Deleted during Execution

Event Type

Debug Tool to Use

IECUBE

E1/E20/EZ Emulator/COM Port

Simulator

Without OCD Trace Function

With OCD Trace Function

8-bit bus width products

Except for 8-bit bus width products

Hardware Break
(before execution)

 

-

-

-

 

Hardware Break
(after execution)

 

 

 

 

 

Hardware Break
(access)

 

-

 

 

 

Software Break

 

-

-

-

-

Trace
(trace start/trace end)

 

-

-

-

-

Point Trace

 

-

-

-

-

Timer Result
(timer start/timer end)

 

-

-

-

-

Action (Printf)

 

-

-

-

-